|
|
|
Microelectronics & Precision Sensors
Formerly SSEC. Providing best value specialized semiconductor
and sensor solutions since 1965
|
|
|
|
|
|
|
|
| Honeywell > DSES > M&PS |
|
Magnetic
Sensors
Global Positioning Satellite Navigation Solutions
| Click Here For Our New Website |
| |
| Honeywell's
Electronic Compass Modules are Used for Compass
Solutions as the Perfect Complement to GPS
Navigation Systems |
| |
Global
Positioning Satellites (GPS) offers the latest
method in high accuracy navigation by using
a constellation of 24 satellites orbiting
the earth and transmitting microwave band
radio frequencies across the globe. GPS receivers
capture at least 4 of the satellite transmissions
and use difference in signal arrival times
to triangulate the receiver's location. This
location information is provided in the classic
latitude (north-south) and longitude (east-west)
coordinates given in degrees, minutes and
seconds. Without a compass, GPS receivers
must collect several sets of coordinates,
or waypoints, and then determine a general
sense of direction of travel. By complementing
GPS receivers with electronic compasses, more
precise and instantaneous headings are provided
to aid navigation for air, ground, and water-based
systems. Electronic map displays can be quickly
updated when combining electronic compass
bearings with GPS receiver derived location
coordinates. Should GPS signals become blocked
due to obstructions or severe weather, the
compass updates and system speed information
can provide a temporary backup in navigation.
Electronic compassing for GPS applications uses Honeywell's magnetic sensors configured for sensing earth's magnetic field at about 0.6 gauss. This natural magnetic field has a direction from the magnetic south pole to the magnetic north pole. By determining the magnetic sensors orientation relative to the south to north pole field direction provides the required heading information. The magnetic sensors measure the magnetic field intensity in a single direction and when two or three sensors are placed at right angles to each other, create a vector summation of the earth's magnetic field. The Electronic compass function takes these sensor inputs, and with trigonometric computation by a microprocessor, calculates a heading relative to the sensor orientations. The heading output is described in degrees with north at zero degrees, east at 90 degrees, south at 180 degrees, and west at 270 degrees. |
| |
| Honeywell
Compass Solutions for GPS Navigation
|
| |
| Honeywell
M&PS offers both
magnetic field sensors and complete electronic
compass modules for electronic compassing.
The HMC102X and HMC105X families of linear
mode magnetic sensors are particularly suited
to cost effective earth's magnetic field measurement
for electronic compassing and navigation purposes.
These magneto-resistive sensors offer miniature
package sizes, high reliability, fast response,
and high sensitivity required for compact
GPS navigation platforms. For more turn-key
compass solutions, Honeywell's line of HMR
compass modules cover a wide range of compass
requirements from the basic HMR3200 two-axis
electronic compass to the HMR-3300 with +/-60
degrees of tilt compensation. Each compass
module has a user calibration routine for
adapting to the location of the compass in
the platform (vehicle, aircraft, ship, etc.).
In addition, each compass module can be ordered
as a development kit with demonstration software
and cabling for personal computer operation.
|
|
|
|
|
|